Produkty a technologie - hledat řešení, dodavatel nebo produkt, nejdůležitější údaje o dodavatelích a vyhledávání produktů, online katalog
   Kontaktujte Vyberte zemi Vyhledat (tipy)  
 Anixter logo  Czech Republic
  
    
 
  
   Seřazeno dle:
> Přehled
> Řešení kabeláže pro firmy (+/-)
> Zabezpečovací technologie
> Kabely & vodiče
> Upevňovacie prvky & komponenty triedy 'C'
> Přehled dodavatelů
> Případové studie


 Najdi produkty:   

 Zobrazte si váš účet:   

Tel: +420 272 181 000
 Přeji si být kontaktován
 specialistou z Anixteru

Výrobky >> Patchsee
Vendor/PatchSee/Overview

From an idea to a product meeting a real need

PatchSee was created in January 2001 with the launching of the light identification RJ45 patch cords and cables on the telecommunications market. The company has since experienced considerable growth in sales.

Right from the start, PatchSee adopted an aggressive export sales strategy, especially on the main European markets.
Exports now account for more than 45% of sales.

Extensive work with the network professionals inspired PatchSee to invent the world's first cable integrating fibre optic technology (patented internationally) for maintenance and mamagement purposed.
PatchSee presents thus an innovative solution to manage your information Network : Intelligent Patch Cords RJ 45 with plastic optical fibre, integrated into the cable. This inventive concept combines practicality, respect for international technical standards, rigorous quality control and prompt service, all of which contirbute to PatchSee's international success.

One of the concerns of the network administrators is to identify and quickly find the patch cord in a cabinet that contains easily more than hundreds of them! This France based company integrated two plastic optical fibres running through RJ45 cables length so that each extremity can be identified.
A simple, reliable and effective solution which granted PatchSee their first succes in France and is now being sold through Anixter in several other European Countries.

Used in over 4 million cables installed around the world, PatchSee Optical Technology gives IT managers a proven solution for handling their everyday cable identification needs.

Identify your cables at Light Speed.

No documents found


 

<<Zpět Poslat tuto stránku>>  Verze pro tisk

   
  Prohlášení o ochraně soukromí  |  Podmínky a ustanovení  |  Kontaktujte nás  |  Doplňující webové stránky  |  Vztahy s investory  |  ©2006 Všechna práva vyhrazena