ESM maximizes uptime of your exacqVision enterprise recorders

(INDIANAPOLIS) — Exacq Technologies, part of the Security Products business unit of Tyco (NYSE: TYC), a leading manufacturer of video management system (VMS) software and servers used for video surveillance, has released the new Enterprise System Manager (ESM), a powerful, browser-based health monitoring system for exacqVision video security systems.

 

The ESM server software monitors the health and status of exacqVision servers and cameras on the network. Users can monitor their exacqVision systems via the intuitive ESM dashboard interface through most web browsers running on a computer or mobile device . With the ESM application, exacqVision users instantly receive an email notification in the event of system errors or warnings, resulting in maximum uptime of servers and red uced software maintenance time. ESM features more than 25 user-defined warnings that can be selected including recorder offline, storage warnings, drive failures, temperature alerts and camera disconnected.

 

In addition, the new ESM software enables end us ers to schedule software updates for hundreds or thousands of recorders during non-peak hours. This significantly minimizes business interruptions and reduces software maintenance time.

 

ESM is supported on exacqVision systems with an exacqVision Enterprise VMS license. This includes an IP camera utilizing the exacqVision Edge software, which allows it to operate as both an IP camera and an exacqVision server.

 

For more information on the new exacqVision ESM and other new updates and offerings, go to www.exacq.com.

 

About Exacq

 

Exacq Technologies is part of the Security Products business unit of Tyco (NYSE: TYC), the world’s largest pure-play fire protection and security company. Exacq Technologies  designs and manufactures the cross-platform, open-architecture exacqVision video management system (VMS) used in the physical security industry for IP video surveillance. exacqVision is available on factory-installed hybrid and IP camera servers or on commercial off-the-shelf servers. It can also be installed directly on compatible IP cameras, eliminating the need for a separate server. Video from exacqVision servers can be accessed with the free, cross-plat from (Windows/Linux/Mac) client, most web browsers and via the free exacq Mobile app available for iPhone, iPad and Android devices. Exacq’s products are available throughout the world.

 

Tyco Security Products and its leading brands conducts business in over 177 countries around the world, in multiple languages and employs over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more, and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential. Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world’s top 100 retailers, over two million commercial enterprises, thousands of students in more than 900 educational facilities, and over five millionprivate residences.