BERK-TEK

line break
Berk-Tek

Berk-Tek, A Nexans Company, is a world-class manufacturer focused on delivering cabling excellence. For more than 50 years, Berk-Tek has been a leading manufacturer of network copper and fiber optic cable products.

The company has led in the development of high-performance and enhanced fiber optic and UTP cables designed to transport high-speed data and voice transmissions for the LAN, Data Center, and Security markets. Berk-Tek proudly manufactures in the United States with manufacturing facilities in New Holland, PA. and Fuquay-Varina, NC.

Berk-Tek, a Nexans company, and Leviton announced a long-term strategic agreement, creating the Berk-Tek Leviton Technologies alliance. The combined strength of Leviton’s extensive connectivity portfolio with the leading performance of Berk-Tek’s cables creates the industry’s premier copper and fiber solution that provides customers with a best-of-breed option for reliable and high-performance networks. Learn more at www.berkteklevitontechnologies.com.

 

Upcoming Webinars

banner

The Berk-Tek webinar, Going the Distance: Innovative Ways to Extend Your Network, will present several solutions for maintaining the reach you need for maximum performance while supporting an ever-increasing amount of bandwidth over your network. Attend this webinar if you want to learn about:

  • The evolution of the fiber backbone
  • Wireless requirements for up to 40G in new construction
  • The distances you can reach with different multimode fibers
  • A unique Berk-Tek solution for indoor/outdoor applications

According to the Cisco VNI forecast, global IP traffic is expected to nearly triple between the years 2015 and 2020. As buildings become more connected and more intelligent, data traffic will continue to increase exponentially. Installing Cat 6A solves the bandwidth challenge in the horizontal. But what about the fiber backbone that needs to support all of those additional 10Gbps drops? And how about wireless access points or security cameras in the parking garage that far exceed the 100 meter distance limitation?

 

WHEN: June 26, at 2:00 p.m. ET

Recorded Webinars

These webcasts are aimed at explaining how emerging technologies will impact the network infrastructures currently in place and under development. Berk-Tek is focused on preparing you to create the resilient network that enables organizations to achieve a maximum usable network lifespan by providing insight into relevant standards and technologies.