Routing Guide Archive

Anixter's U.S. Domestic Freight Routing Guide Older Updates

  • 12/14/15: Updated LTL routing guide to reflect change to 3rd party billing address for Conway shipments. All 3rd party billing will now go to the same address.
  • 11/20/15: Updated LTL routing guide to reflect the XPO/Conway merger. All lanes formerly with Conway are now with "XPO formerly Conway".
  • 3/30/15: Updated LTL routing guide for inbound shipments to the states of IL, KS, MI, MN, and OH. See attached guide for changes.
  • 11/10/14: Updated inbound routing guide to the state of MO. All freight from the following states into the state of MO are now Dayton Freight: IL, IN, IA, KS, KY, MI, MN, MO, OH, WI.
  • 9/1/14: Updated inbound routing guide for shipments out of the following states for specific lanes: IN, MI, NJ, OH, PA, VA, WV. For all shipments out of these states, please refer to routing guide for specific changes.
  • 7/7/14: Updated inbound routing guide for the following lanes: IL to IL and MI will now be Dayton Freight. MI to IL, IN, MI, MO and OH will now be Dayton Freight.
  • 11/22/13: Updated outbound routing from the state of IL to the states of DE, IL, IN, MD, NJ, OH, PA, VA and WV to reflect (Chicago Only - Pitt Ohio) FedEx Freight Priority. Unless shipping out of the Chicagoland areas of IL, FedEx Freight should be used when shipping out of IL.
  • 3/18/13: Updated inbound routing to the state of IL from DE, IN, MD, NJ OH, PA, VA, WV to reflect (Chicago Only - Pitt Ohio) FedEx Freight Priority. Unless shipping to the Chicagoland areas of IL, these states will use FedEx Freight Priority.