AXIS Q3517-LV and AXIS Q3517-LVE Fixed Dome Network Cameras

AXIS Q3517-LV and AXIS Q3517-LVE Fixed Dome Network Cameras image

The AXIS Q3517-LV/-LVE cameras will be addressing the need for monitoring in multi-megapixel detail at full frame rate with the best video quality on the market, including Forensic WDR, enhanced Lightfinder, OptimizedIR and Zipstream technology, along with a range of further top-of-the-line capabilities. Solid performance - these new top-of-the line AXIS Q35 cameras offer unparalleled video quality in harsh environments at any light conditions, and further great capabilities that support the surveillance assignment.

Key Features

  • 5 MP resolution at full framerate
  • Forensic WDR, Lightfinder and OptimizedIR
  • Axis Zipstream technology
  • EIS and vandal resistance with IK10+ rating
  • Power with redundancy and configurable I/O ports