Berk-Tek Transceiver Banner image

Introducing Berk-Tek's complete line of optical transceivers now available in a variety of form factors and transmission speeds, including 1Gb, 10Gb, 40Gb, 8Gb FC, and 16Gb FC.

Berk-Tek Transceiver image

When you source your transceivers from a trusted Layer 1 partner like Berk-Tek, you Own the Link.  And when you pair Berk-Tek’s premium transceivers with GIGAlite™-10XB glass, you will see the difference when you need longer reach and/or more connections than the standards allow - GUARANTEED.

CONSISTENT, RELIABLE SUPPORT

Traditionally, transceivers have been purchased from equipment manufacturers. Since a transceiver’s performance has more to do with the cabling than the equipment, shouldn’t the cable and transceivers be specified together? This simplifies the supply and maintenance of the entire link. No more calling the switch or server manufacturers if you need support. With Berk-Tek transceivers, you can own the entire link.


MAXIMUM FLEXIBILTY & SCALABILTY

Ever-increasing bandwidth demand is driving changes to your network and data center. Rest assured that in the coming years, you will need more servers, more switches, and more storage capacity connected at higher data rates. Using Berk-Tek’s 40Gbps transceivers paired with GIGAlite™-10XB glass, there's enough power budget to support a link distance of up to 500 meters. Standard compliant solutions offer only 150 meters. Of course, you can trade off distance for more connections, but you have the flexibility to scale your network and data center to whatever your current and future needs require.

Berk-Tek Transceivers Difference image

MAXIMUM FLEXIBILTY & SCALABILTY

Ever-increasing bandwidth demand is driving changes to your network and data center. Rest assured that in the coming years, you will need more servers, more switches, and more storage capacity connected at higher data rates. Using Berk-Tek’s 40Gbps transceivers paired with our GIGAlite™-10XB glass, we guarantee enough power budget to support a link distance of up to 500 meters. Standard compliant solutions offer only 150 meters. Of course, you can trade off distance for more connections, but you have the flexibility to scale your network and data center to whatever your current and future needs require.

Related Documents

  • CASE STUDY - Large nationwide bank looks to Berk-Tek to help redifine the link, improve processes, and streamline operations. 
  • WHITE PAPER - Optical Fibers, Transceivers and Connectivity – A New Perspective 

berk-tek transceivers image