Latest version also includes advanced camera configuration options, new IP camera integrations and more

(INDIANAPOLIS) —Exacq Technologies, part of the Security Products business unit of Tyco (NYSE: TYC), has made searching for video surveillance evidence faster and more intuitive with the new Speed Search feature in exacqVision 6.0 — the latest release of the company’s Video Management System (VMS) software. exacqVision now also makes it easier to configure IP compatible cameras from the exacqVision client. Included with this release are updates to the Exacq Mobile app, the exacqVision web client and Enterprise System Manager (ESM), a health monitoring program for use with exacqVision NVRs.

 

With SpeedSearch, video frames automatically populate on the screen upon conducting a search and advance as the timeline cursor is moved. “SpeedSearch allows users to start investigating video while it’s still downloading, providing faster access to the evidence they need,” notes Tom Buckley, Vice President of Sales and Marketing, Exacq Technologies. “It’s also ideal for low bandwidth connections as investigations can occur with out having to wait for an entire video stream to download.”

 

With the release of version 6.0, the exacqVision VMS now supports over 1,800 IP camera models from the industry’s leading manufacturers including ACTi, American Dynamics, Arecont Vision, Axis Communications, Bosch, Canon, IQinvision, JVC, Panasonic, Pelco, Samsung, Sony and Vivotek. The exacqVision VMS software and servers also integrate with access control systems, retail analytics and video analytics systems, allowing professional integrators and end users to create a complete, best-of-breed IP video surveillance solution.

 

The latest Exacq Mobile app (Version 3.4) allows users to search multiple cameras simultaneously from the same screen. In addition, users can now browse all available cameras from multiple servers on one list or browse cameras arranged by server. The ability to view de-warped video from panoramic or fisheye cameras has also been added to this latest release.

 

The exacqVision Enterprise Server Manager (ESM) allows users to maximize the uptime of large exacqVision deployments while reducing overall administrator maintenance time. The latest release of ESM (Version 2.4) adds the ability to easily track the days of storage available on exacqVision servers. It also adds a new interactive help guide, which explains all of the monitoring features available within the system.

 

The exacqVision VMS is accessed with the freely distributed exacqVision client software (Windows/Linux/Mac), the exacqVision free web client available for all leading web browsers (Google Chrome, Firefox, Internet Explorer, Safari and Opera), as well as the free Exacq Mobile app for iOS, Android and Windows Phone 8 devices. The VMS software is included with pre-configured exacqVision NVR servers or it can be installed on third-party Windows or Linux based systems.

For more information on this exacqVision software release and other new updates and offerings, go to www.exacq.com.

 

About Exacq

 

Exacq Technologies is part of the Security Products business unit of Tyco (NYSE: TYC), the world’s largest pure-play fire protection and security company. Exacq Technologies designs and manufactures the cross-platform, open-architecture exacqVision video management system (VMS) used in the physical security industry for IP video surveillance. exacqVision is available on factory-installed hybrid and IP camera servers or on commercial off-the-shelf servers. It can also be installed directly on compatible IP cameras, eliminating the need for a separate server. Video from exacqVision servers can be accessed with the free, cross-platform (Windows/Linux/Mac) client, most web browsers and via the free exacq Mobile app available for iPhone, iPad and Android devices. Exacq’s products are available throughout the world.

 

Tyco Security Products and its leading brands conducts business in over 177 countries around the world, in multiple languages and employs over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more, and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential. Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world’s top 100 retailers, over two million commercial enterprises, thousands of students in more than 900 educational facilities, and over five million private residences.