Enable a Safer Workplace with Touchless Access Control Solutions from HID Global

HID Touchless Access Control Solutions

As organizations around the world decide how and when to safely return to the workplace, one common factor is clear — reducing touchpoints between people and objects is key.

HID Global Logo

Access control solutions from HID Global, such as HID Mobile Access®, HID® Signo™ Readers, and HID Location Services, can be used to enable touchless entry to facilities, reduce person-to-person contact via over-the-air credentialing, and provide real-time building occupancy data to help with compliance and social distancing. These solutions can help accelerate a return to work and speed economic recovery.

  • HID Mobile Access: Reducing physical touchpoints is made easy with HID Mobile Access. Compatible with hundreds of mobile devices, employees can access facilities and more without needing to physically touch cards or readers. Additionally, over-the-air credentialing removes the need for person-to-person issuance for both employees and visitors.
  • HID Signo Readers: Security meets modernity with HID Signo, the signature line of access control readers from HID Global. HID Signo Readers are highly versatile supporting the widest range of credential technologies, including HID Mobile Access via native Bluetooth and NFC capability.
  • HID Location Services: HID Location Services combines a hardware and software solution that delivers actionable occupancy data that scales and expands based on the need of the facility. To provide insights in real time, HID Location Services offers live building occupancy information at the room and floor level, including the ability to create alerts to meet social distancing requirements.

 

Eligible Items

MID-SUB-T100

MID-SUB-T100 | 1YEAR USER LICENSE FOR HID ORIGO MOBILE IDENTITIES

40NKS-00-000000

40NKS-00-000000 | Signo40, Wall mount, 13.56mHz &125kHz, OSDP/Wiegand, Pigtail, Mobile Ready

BVSPUS-PACS

BVSPUS-PACS | HID Location Services Starter Pack US Version