Introducing AXIS P32 MK II Fixed Dome Network Cameras

AXIS P32 MK Fixed Dome Network Cameras image

Axis Communications is pleased to announce the launch of the new AXIS P32 MK II Fixed Dome Network Cameras.

All current AXIS P32 models will be discontinued and replaced by the new AXIS P32 MK II models. The AXIS P32 MK II cameras offer outstanding image quality with WDR – Forensic Capture, Lightfinder, and some models with built-in IR illuminators. The affordable, reliable AXIS P32 cameras with remote zoom and focus are easy to install and provide an efficient way of adjusting the field of view if needed. All models support Axis’ Zipstream technology, which implies significantly reduced bandwidth and storage needs allowing for great cost savings. The AXIS P32 Series offers attractive and affordable alternatives to the AXIS P33 and AXIS Q35 Series. 

Models

Related