NEC Display Solutions Delivers New Options with the Launch of the C Series Commercial - Grade Displays

banner

C Series displays from NEC Display Solutions bring thin depth, commercial controls, and professional performance
to a higher level for cost-conscious users.

Thin Depth

image

Full External Control

image

Commercial Grade

image

This slender profile (45mm total depth) allows for lighter design and unobtrusive mounting capabilities giving maximum accessibility in hallways and corporate environments where ADA compliance is of utmost importance.

Bidirectional external control through RS232 and LAN allow for easier implementation of these products into existing control systems and also allow for the necessary feedback for asset tracking.

The display can be used in both landscape and portrait installations, expanding the ways in which users can deploy them and contains an anti glare screen that will allow for maximum readability of the on-screen content by reducing the reflectivity of ambient light.