Milestone Logo

Milestone Husky network video recorders (NVRs) now make the analog-to-IP evolution easier and more affordable than ever with encoders built into new hybrid models.

Milestone Systems, the open platform company in IP video management software (VMS), is announcing an easier and more affordable way to make the transition from analog to digital technology. There is no need to throw out older cameras that are still working, as you add new network devices to your surveillance solution.

 

The Milestone Husky™ series of NVRs will now offer versions with integrated encoders that make it simple to connect analog and digital cameras, which run on IP networks, to the same box. Milestone Husky Hybrid NVRs are preinstalled with Milestone VMS and let end users build on their initial investment. The end users can continue to use existing analog cameras and add IP cameras over time for better evidence-quality video and surveillance features.

 

The Milestone Husky Hybrid NVRs are aligned with the new Milestone encoder licensing. In this only one hardware device license is needed for each analog-to-IP encoder, regardless of the number of analog cameras connected to the encoder. This applies to encoders with no more than one IP license. The Milestone Husky Series also supports the Milestone encoder licensing when external encoders are used on the NVRs.  End users can choose from more than 200 encoders.

 

At launch two configurations of Milestone Husky Hybrid NVRs will be pre-installed with XProtect 2014:

  • Milestone Husky M30 Hybrid with 16 analog channels + 4 IP devices 4 TB storage / 8 GB RAM / i5 processor

  • Milestone Husky M50 Hybrid with 32 analog channels + 16 IP devices 6 TB storage / 16 GB RAM / i7 processor

General availability is fall 2014 in the U.S., Europe and the Middle East.

 

Read the full article here.

Milestone Husky NVRs Available Now at Anixter

Request a quote from Anixter today!

Huksy M30
Husky M50