OneAdvisor-1000

400G High-Speed, Portable Network Tester

ONA1000_Anixterbanner_960x150

The OneAdvisor-1000 delivers all the test capabilities technicians and engineers need to install and maintain high-capacity networks. Supporting emerging and legacy technologies, the OneAdvisor-1000 is ideal for metro/core, data center interconnect, and business services testing. OneAdvisor-1000 uses the same user interface and workflows as the other T-BERD/MTS products.

Overview

The industry’s most comprehensive tool for 400Gbps testing provides multi-protocol coverage to address service activation, troubleshooting, and maintenance. The portable tester provides the latest technology with interfaces such as QSFP-DD and SFP-DD. The OneAdvisor-1000 provides rate integration to cover 400GE testing in addition to fiber optic testing using OTDRs. The supported combinations provide investment protection by covering future technology and the possibility to cover legacy protocols. With advanced tests like Optics Self-Test for QSFPx pluggables, RFC 2544/Y.1564, and OTN Check, technicians can test their networks faster and more accurately than ever before.


t-berd-mts-400g

Key Features

  • PAM-4 native support provided via connectors and interfaces also to test 400GE
  • QSFP-DD and SFP-DD interfaces
  • Compatible with fiber optics test modules such as OTDR and WDM Channel Checkers
  • Tests new technology including PAM-4 and KP4 FEC at 400GE
  • Scalable and Modular

Benefits

  • Optimized for central office use with a 10-inch multi-touch screen, scripted workflows, and clear pass/fail results 
  • PAM4 native support provided via connectors and interfaces to test 400GE 
  • Simplifies multi-technology testing via modularity to provide an all-in-one solution 
  • Compatible with fiber optics test modules such as OTDR

Related Resources