Pelco Introduces Next Generation of Sarix Professional Cameras
Pelco logo

CLOVIS, CALIF. – April 27, 2016 – Pelco by Schneider Electric, a leading provider of intelligent video surveillance and security management platforms, announced enhancements to its Sarix™ Professional camera line. The upgrades enable users to capture high-quality imagery to enhance security, safety and operational strategies.

With resolutions of 1.2MP to 5MP, the Sarix™ Professional range of surveillance cameras deliver high-resolution images while providing video coverage of larger areas with a single camera. Sarix advanced zoom capability allows operators to see detailed scenes for evidentiary purposes, supporting faster and more efficient investigations.

The superior low-light performance and adaptive infrared (IR) illumination captures important details in the dark, such as faces and license plates that are critical for effective site security and asset protection. When light sources are not present, Sarix Professional dynamically optimizes exposure settings to capture the finest details in reduced lighting scenarios. With the exception of the micro dome model, Sarix Professional cameras are vandal resistant to IK10 and therefore ideal for locations where security equipment could be at risk.

New features of the Sarix Professional camera range include:     

Sarix® IJP Series Indoor Micro Dome
  • Edge Storage: Sarix incorporates onboard edge storage with a micro SD card. Video clips of varying lengths can be stored to the card upon alarm or video can be written continuously to the SD card in the event of a network outage. Video can be retrieved from the card through the FTP protocol or by using an ONVIF Profile G-enabled client.
  • Analytics: The camera line contains a built-in motion detection algorithm that allows it to record or send an alarm when motion is detected in a selected zone or within the entire scene. A camera sabotage alarm is triggered if the lens is obstructed or when the camera is repositioned, proactively informing operators of any potential tampering issues.
  • Open and Integrated: The cameras seamlessly connect to Pelco video management systems such as VideoXpert™Endura® version 2.0 and Digital Sentry® version 7.3 Pelco Sarix Professional cameras also integrate with major third-party systems through the open Pelco API, or the ONVIF Profile S and Profile G standards.

Sarix Professional Range Brochure

Product Specifications

 Pelco has long been known for the superior quality of our video surveillance solutions, and the updates we’ve made to our Sarix Professional camera line deliver users with increased video capture functionality and image clarity. Sarix Professional’s extensive benefits, combined with excellent video quality at a competitive price, make it the definitive camera for a wide variety of security environments. 

Doug Ringer, Senior Product Manager, Pelco by Schneider Electric

Related