CommScope In-Building Wireless | Wired for Wireless®

CommScope In-Building Wireless DAS

CommScope's Wired for Wireless Solution is a cost effective solution designed to allow Enterprise customers to prepare their buildings for wireless coverage. By deploying broadband coaxial cable and antennas throughout a building during the construction phase, custom design is eliminated and system costs are lower. The solution paves a path for the in-building wireless needs of today and tomorrow.


CommScope's Wired for Wireless Solution includes coaxial cables, connectors, antennas and cable management apparatus, connected together in such a way as to provide ubiquitous wireless coverage through the entire structure.


Unique Wired for Wireless guidelines for antenna placement eliminate the need for costly and time consuming RF site surveys and protects the wireless performance inside the building from the future changes of the outdoor network.


CommScope's future-proof and cost-effective platform for uniform coverage will meet the ever increasing indoor wireless requirements. CommScopes Wired for Wireless Solution has the Enterprise Covered.

Wired for Wireless Solution Components

High performance indoor antennas, coaxial cables, connectors, and cable management apparatus ensure that the Wired for Wireless Solution delivers a cost and performance optimized platform that is ready for carrier-neutral and uniform wireless coverage in Enterprise buildings.

In-building Wireless DAS Omni-directional Antenna

Cell-Max™ Omnidirectional Antenna
The CELLMAX-O-CPUSE antenna is a ceiling mounted omnidirectional indoor antenna designed for the 698-960 MHz and 1710-2700 MHz frequency ranges. It supports all modulation formats and technology including, Analog, iDEN, GSM, GPRS, EDGE, UMTS, HSDPA, HSUPA, LTE, CDMA2000, EV-DO, Wi-Fi, Wi-Max and many more.

In-Building Wireless DAS Directional Antenna

Cell-Max™ Directional Antenna
The CELLMAX-D-CPUSE antenna is a wall mounted directional indoor antenna designed for the 698-960 MHz and 1710-2700 MHz frequency ranges. It supports all modulation formats and technology including, Analog, iDEN, GSM, GPRS, EDGE, UMTS, HSDPA, HSUPA, LTE, CDMA2000, EV-DO, Wi-Fi, and Wi-Max and many more.

CommScope DAS FXL-540-NHR HELIAX cable

FXL-540-NHR HELIAX® cable
The FXL-540-NHR cable is a flexible inch 50 ohm coaxial cable, with a black PE jacket, a smoothwall aluminum outer conductor, foam PE dielectric and a copper clad aluminum inner conductor. With its light-weight and cost effective construction, the FXL-540-NHR cable is easy to install and delivers excellent transmission performance.

CommScope EZFit® Connector for FXL-540-NHR cable

EZFit® Connector for FXL-540-NHR cable
The 540EZNMV2 EZFit connector is a high performance N-type male connector that is a perfect match for the FXL-540-NHR cable. The 540EZNMV2 is a small and lightweight two piece connector designed for easy installation and optimal electrical performance. High precision cable preparation and 540EZNMV2 connector attachment is achieved with the 12-HPT EZFit hand prep tool or the 540-ZPT EZFit drill prep tool.

CommScope AL4RPV-50 HELIAX® cable

AL4RPV-50 HELIAX® cable
The AL4RPV-50 cable is a flexible inch 50 ohm plenum rated coaxial cable, with an off-white PVC jacket, a corrugated aluminum outer conductor, a PE Spline air dielectric and a copper clad alumimum inner conductor. With its light-weight and cost effective construction, AL4RPV-50 cable is easy to install and delivers excellent transmission performance.

CommScope Positive Stop™ Connector for AL4RPV-50 cable

Positive Stop™ Connector for AL4RPV-50 cable
The L4TNM-PSA Positive Stop connector is a high performance N-Type male connector that is the perfect match for the ALPRV-50 cable. The L4TNM-PSA Positive Stop connector is a small and lightweight connector designed for ease of installation and optimal electrical performance. The L4TNM-PSA connector can be installed with standard tools. Cable preparation for L4TNM-PSA connector attachment can be achieved with MCPT-L4 EASIAX manual cable prep tool or the drill-assisted EASIAX Plus CPT-L4ARC1 automated cable prep tool.

Ask an expert


Talk to an In-building Wireless Expert