PROGRESS LIGHTING

line image
Progress Lighting logo

Progress Lighting is the largest single source for residential and commercial lighting, offering more than 5,000 lighting fixtures and is committed to providing a diverse selection of high quality lighting fixtures - earning them the reputation as the number one decorative lighting line among builders and remodelers. Specialties include: residential lighting, (multi-family) residential lighting, and (light) commercial lighting.

Area/Site

Progress Lighting Area/Site Lighting image

From parking lots to pools, Progress Lighting’s energy efficient outdoor products create a well-lit environment with low maintenance benefits.

Exit/Emergency

Progress Lighting Exit/Emergency Lighting/Signs image

Progress Lighting’s LED exit signs and emergency lighting units, that include remote emergency lights, battery packs and central lighting inverter options, address a wide range of commercial applications to enhance safety and ensure security in your facilities.

Linear/Troffer

Progress Lighting Linear/Troffer Lighting image

Adding general and task lighting to multi-purpose areas, including, stairwells, laundry areas, common rooms, offices and more can be done beautifully and efficiently with low profile linear and troffer options. And because they feature LED and CFL sources, you’ll enjoy energy cost savings.

Decorative Fixtures

Progress Lighting Indoor Lighting image

Overhead lighting, sconces, hanging, bath and vanity fixtures provide general illumination for interior spaces in apartment communities, townhomes, mixed-use residential facilities and more. Decorative LED and CFL options reflect the latest design trends, while also providing energy efficient benefits.

Recessed

Progress Lighting Recessed Lighting image

Designed to fit in small spaces and provide accent or task lighting, Progress Lighting’s undercabinet offering features a subtle – yet wide distribution – under kitchen cabinets, on bookshelves, in display cases, alcoves and more.

Undercabinet

Progress Lighting Undercabinet Lighting image

Designed to fit in small spaces and provide accent or task lighting, Progress Lighting’s undercabinet offering features a subtle – yet wide distribution – under kitchen cabinets, on bookshelves, in display cases, alcoves and more.

This is Progress Brochure image

This is Progress

With more than 110 years as a lighting manufacturer, our heritage is rich with historical insight and experience. However, we are not resting on our past. Progress Lighting has a new illuminating vision, one that concentrates on solutions and affordability.

2017 Product Catalog image

2017 Product Catalog

Progress Lighting is more than just a lighting manufacturer with a rich heritage. They are illuminating a vision for the future. Celebrating more than a century of successful partnerships, Progress Lighting turns their focus to the future in creating collections that highlight affordable luxury lifestyles throughout homes nationwide.

Progress Lighting Commercial Lighting Brochure image

Progress Lighting Commercial Lighting Brochure

The Progress Commercial Lighting catalog is a complete solution for light commercial projects. Their recently expanded offering includes light commercial and commercial luminaires that work together to provide a unique solutions approach to a variety of multi-use applications, including multi-family, hospitality, assisted living – and many others.

Title 24 Brochure image

Title 24 Brochure

Title 24 is enforced by the building or electrical inspector at the site of the lighting installation and may involve the homeowner, contractor and/or builder. The building permit process is used to identify and track compliance. If a lighting installation is noncompliant as installed, an occupancy permit maybe delayed or denied. Use this guide to select T-24 compliant products for your next project.

Featured Progress Lighting Products

Progress Lighting PE2EU Series LED Emergency Light image
Progress Lighting PECUE Series LED Combination Exit/Light image
Progress Lighting P8022 Series 7.25 inch LED New Construction and Remodel | Wet Location image
P5299-31LED Landscape Flood Light image
P6832-2030K Step Light/Wall Light image
P560052-020-30 Callahan LED Outdoor Wall Lantern image