TALKAPHONE

Talk a phone

Talkaphone, a WESCO-Anixter Solutions Partner, is the industry’s leading designer and manufacturer of security and life safety communication products and solutions for customers all over the world. Known for the best quality, technology and solution for every need and budget, Talkaphone is committed to being the best to work with.

Talkaphone has been in business for more than 85 years. They originally made their name supplying mission-critical communication equipment to the military and defense industry. Since then, they have grown and thrived through continuous innovation, becoming the leaders in safety and security communication as their customers’ needs have evolved.

Featured Talkaphone Products

AOR-IP-40-CU | Area of Rescue IP Command Unit with 40-Station Capacity
AOR-IP-80-CU | Area of Rescue IP Command Unit with 80-Station Capacity
VOIP-201C-WAV1 | Compact IP Call Station with CALL signage and WaveSense touchless sensor
VOIP-201C3-WAV1 | Compact IP Call Station with CALL signage, built-in IP camera, and WaveSense touchless sensor
AC-BP-1 | Biometric Screening Panel for Access Control