Introducing the Oberon's 905 Series

Locking AP surface mount for wall and hard ceilings


Oberon’s H-Plane Model 905 mounts and secures Cisco and HP Aruba Wi-Fi Access Points directly on the wall or hard ceiling.

The 905 can be mounted directly over a wall outlet. Its AP-specific hinged cover recesses the access point into the box for a low-profile, aesthetic appearance. Doors are available for additional AP models on request.

Simple & Secure Cabling

Cabling is terminated inside the 905, and the 905 locks and secures both access point and cabling. The 905 also has knockouts for jack modules to provide network plug-in locations.

Eligible items

Aruba AP515/514
Cisco 9130AXI