New NSE Version 8.14 Delivers Enhanced Bandwidth Functionality for Visitor-Based Networks

Version 8.14 of the Nomadix Service Engine provides increased flexibility and expansion of bandwidth management, performance gains and simplified operations for the EG 6000.


nomadix-software-release

NSE Version 8.14 is available now for the AG 2400, AG 2500, AG 5900 and EG 6000 Gateways. Key features in this release include:

Distribution of Unused Bandwidth Per Class

Distribution of Unused Bandwidth per Class allows unused bandwidth to be allocated on a per‑class basis. When Unused Bandwidth is enabled for a specific class all unused bandwidth will be proportionally distributed to all devices in a class. If Distribution of Unused Bandwidth per Class is not enabled, all devices will be held to the individual or group bandwidth caps.

Persistent Connections

Persistent Connections for Portal XML Posting allows a single TCP connection to send and receive multiple HTTP(S) requests/responses per connection versus opening a new connection for every single request/response pair. This can result in improved performance.

EG 6000 Password Recovery

NSE Version 8.14 provides a simplified method to recover a forgotten Manager Login Name and Password without requiring a console port. Complete instructions can be found in the EG 6000 Cabling and I/O Interface Guide.