Sustainability must roll forward faster

Panduit Logo

At last, almost everyone agrees that the world’s environment is in crisis. Governments, industries, corporations, down to individuals are now taking steps towards better environmental stewardship. We must all take responsibility for our actions and help reduce the CO2 emissions we create and work to achieve Net Zero.

Michael Akinla

(By Michael Akinla, Panduit Business Manager, Northern Europe, and Ireland)

Original article from digitalisationworld.com

Suppliers, customers, investors, and employees all understand that this is not an easy path, but it is an essential one. We have all witnessed, over the past decade, how the data centre industry has grown from an obscure market to a key economic engine for every developed and developing country. The data centre industry continues to grow and with it the need to reduce the negative environmental impact generated, from the construction phase, through fit out, to resource utilisation, such as, water and energy and back through the supply ecosystem.

 

At Panduit, they concentrate on delivering the physical ITE infrastructure to data centres, enterprise and industry and environmental stewardship is part of a holistic approach to the company’s business philosophy. They have realised that customers recognise that sustainability is a key driver for future growth, and they want to partner with companies that are committed to sustainable business practices.

 

 

Panduit, like many organizations have implemented a broad strategy of greening our supply, production processes and offices, and this is not a late to market effect of customer pressure. These changes were initiated over a decade ago, demonstrated by Costa Rica manufacturing facility which has been carbon neutral certified since 2014. The plant was recognised as a pioneer in CO2 reduction at the 2019 PreCOP25 International Climate Conference.

A key goal is to recycle thousands of metric tons of manufacturing waste per year and reduce Panduit’s carbon footprint by 20% by 2025. A further manufacturing goal is to reduce energy intensity (kWH/Earned Hours) by 10% by 2025, across the facilities.

 


 

Cooling and Air Flow - 37%

  • Energy cost related to cooling accounts for:
    • Nearly 37% of the overall data center power consumption
    • Fastest Rising Data Center Operation Cost
  • Power and cooling capacity remain top targets for efficiency improvements
Cooling and Air Flow

Average data center energy usage allocation

 


 

Manufacturers must make changes in every aspect of their business flows in order to achieve meaningful steps towards Net Zero. Panduit have been reviewing processes across the board, from base materials, manufacturing, transportation, product reuse, recycling, and disposal, all the while innovating to capture, and drive gained benefits forward with new policies and products.

Panduit’s world headquarters was certified as a LEED Gold building. The building’s data centre is cooled by filtered rainwater, and the green roof helps regulate the temperature of the rooms below, while also assisting with rainwater capture. They also harvest daylight using light shelves to bounce natural light into the building to maximise light distribution, which is a subject the R&D teams are very aware of. All these activities generate data, which is used to benchmark, evaluate, and improve the operation of the building’s systems in order to conserve energy, improve occupant comfort, maximise productivity and enhance operations.

Recycling for all

 

Recycling for all

Organizations must be strident in material sourcing. Panduit are RoHS and REACH compliant and have implemented recyclable material packaging. They work with suppliers to upgrade packaging increasing renewable wood and cardboard products as well as recyclable plastic materials.

Like many organisations, Panduit measure, analyse and report the environmental and health impacts of copper cable and connector materials as part of the Environmental Product Declaration (EPD) and Health Product Declaration (HPD) process.

Current investigations include recycling excess fluorinated ethylene propylene (FEP) back into base material and the reuse of copper waste generated from the manufacturing process to achieve 100% waste recycling.

E-Waste is a major challenge according to the Global E-Waste Monitor project. 53.6 Megatons (Mt) of e-waste was generated around the globe in 2019, of this only 9.3 Mt, or 17.4% was disposed of or recycled properly.

Panduit’s R&D Labs have been investigating product efficiency for almost 60-years, helping data centre customers to be more sustainable, whether on-premises or standalone sites, by sharing knowledge and research concerning the amount of energy wasted within infrastructure environment. Up to 40% of data centre energy is used in cooling and lighting, therefore, increasing energy efficiency is important in improving sustainability and reducing carbon emissions.

 

White is right

A number of years ago, Panduit labs undertook research into the benefits of white cabinets compared to black. It found that white cabinets provided a Light Reflective Value of 80% verses black cabinets that offered 5%, this equates to a light energy saving of up to 30%, (1.5-3% of data centre energy), and requiring fewer light fittings in the area. Panduit’s research also found that the reflective light allowed easier working in and around the cabinets for installation and MACs.

An even bigger opportunity to increase energy efficiency is around the servers. ASHRAE TC9.9 has encouraged operators to raise temperatures in technology spaces and introduce environments such as Hot/Cold Aisle Containment Systems that eliminate hot air recirculation. Improving cold air direction into cabinets intake fans reduces inlet air temperature and improves cooling and equipment reliability. Ensuring cabinets are air sealed ensures empty rack spaces and gaps around cable inlets are covered to reduce air leakage by up to 20% and preventing hot air contamination. These measures can reduce energy use by a staggering 40%, a demonstrable sustainability win.

 


 

Lighting - 3%

  • White Cabinets:
    • Light Reflective Value (LVR) 80% vs 5% for Black
    • 25 to 30% light energy savings
  • Increase Visibility inside the cabinet
    • Ambient light sufficient for most work

     

Cooling and Air Flow

Average data center energy usage allocation

 


 

Today, monitoring devices and DCIM systems ensure that data in and around cabinets is collected and reportable to ensure cabinets operate at maximum efficiency, which is good for the data centre, good for customers and good for the environment.

Panduit continues to review product materials and sourcing strategies. Vari-Matrix HD 28AWG patch cords offer the industry’s smallest diameter Cat 6A cable, which uses less material in its manufacture, and maintains the quality and capability of its characteristics. This also allows more cables per bundle around the site and in distribution more reels per pallet, increasing shipping efficiency by reducing the number of traffic journeys. 

 

Panduit continues to review product materials and sourcing strategies.

Companies looking to evaluate potential suppliers should ask for ESG policies and evidence they contribute to internal efficiencies and drive lower energy use, reduction in base materials usage and reduced packaging. Also key, is what internal practices are suppliers taking to drive internal efficiencies to improve sustainability drives, such as EPD/HPD certification on euroclass rated cables which help with LEED and BREEAM and demonstrate a cradle to grave measurement approach