Do you know about LEGRAND UPS?

LEGRAND UPS

Legrand is currently the UPS manufacturer with the highest growth rate on the market.*  The innovative design and high quality of the components used enable their UPS to achieve up to 97% efficiency, leading to significant energy savings.

Legrand

 

*These results have been achieved through actions such as recent acquisitions, product development activity and, above all, growth in sales of products and services.

 

Watch this short video of the Legrand UPS portfolio.

Legrand UPS Distinguishing characteristics

Distinguishing characteristics

High performance - The innovative design and high quality of the components used enable Legrand UPS to achieve up to 97% efficiency, leading to significant energy savings.

Latest generation components - In-depth research on the best electronic components on the market combined with state-of-the-art manufacturing methods, make Legrand UPS extremely reliable and abreast of the times.

Environmentally sustainable products - Efficient UPS built with maximum attention to detail. Moreover, Legrand has developed an innovative testing system which reduces the energy consumed for each device manufactured.

Advanced technology - The On-line Double Conversion technology ensures a top-quality power supply and maximum energy efficiency.

Reliable electronics - The optimum sizing of the power stages and thorough testing of each unit ensure excellent reliability.

High performance batteries - The batteries supplied with Legrand UPS are the best on the market. The innovative charging system significantly extends the life of the battery by up to 50%. 

 

 

Environmental Sustainability

Sustainable UPS: "Turn It green!"

Sustainable UPS:
"Turn It green!"  

2030 Goal = Continue reducing the energy footprint

In a world where resources are limited, we all need to consider the consequences of our actions, our choices, and our work.  Hence, Legrand’s commitment to increasing the sustainability of their UPS’s.

Eco-friendly concepts are integrated throughout the entire product lifecycle; from the design, through the marketing and use phase, and to the disposal phase, leading to a reduction in the environmental impact of the entire system.

 

Key Facts & Figures

  • 10 million tons of CO2 emissions avoided since 2014 
  • 90% of waste recovered
  • More than 2 200 PEP eco-passports are now available for Legrand products  
  • 67% of sales in 2019 were covered by products with eco-passports 
Legrand Single-Phase UPS

Single-Phase UPS

Keor DC

Keor DC

Overview: This UPS is designed to provide the continuity of operation in case of power failure to all Internet connected devices such as modems, routers, cordless or VoIP phones. Its elegant and modern design, with ultra-compact dimensions, allows it to adapt perfectly to the home, even in small spaces.

Key Verticals: Modem, Router and Connected Devices, Small Office, Home Office

Download Brochure

 

Keor Multiplug

Keor Multiplug

Overview: This UPS provides the user with interactive line technology. It delivers a rated power of 600VA and 800VA.  It is CPU-controlled, and it is equipped internally with valve-regulated, hermetically sealed, lead accumulator battery.  The presence of an electronic stabilizer (AVR) inside the UPS provides the connected loads with effective protection against any interference in the electrical mains.

Key Verticals: Home Office, Small Office

Download Brochure

 

Keor SP

Keor SP

Overview: This UPS provides the user with line interactive technology. It delivers a rated power of 600-800-1000-1500-2000VA, it is CPU-controlled and is equipped, internally, with valve-regulated, hermetically sealed lead accumulator batteries. The presence of an electronic stabilizer (AVR) inside the UPS provides the connected loads with effective protection against any interference in the electrical mains.

Key Verticals: Home Office, Small Office and IT Applications to backup computers, network switches, and telecom/faxes.

Download Brochure

 

Keor PDU

Keor PDU

Overview: This UPS is designed for installation in 19-inch panels and racks. It’s a PDU-style format with ultra-compact dimensions.  It provides 8 sockets with up to 15-minute autonomy in just 2 rack units.

Key Verticals: Home Office, Small Office and Applications Related to Voice / Data / Image, Security, CCTV and Network Cabling Racks.

Download Brochure

 

Daker DK Plus

Daker DK Plus

Overview: This is a single phase, uninterruptible power supply with high frequency PWM technology and double conversion online. It delivers a rated power of 1000-2000-3000-5000-6000-10000VA and it is equipped with valve regulated, hermetically sealed, accumulator batteries. These batteries are contained in a specific compartment inside the UPS or, in one or more external cabinets. With the reversible screen, the Daker DK Plus can be used in both tower and 19-inch rack configurations.

Key Verticals: Small and Medium Business, IT Applications, Networks, Servers, Telecom

Download Brochure

 

Keor SPE (coming soon)

For Small and Medium Business, Industrial Applications, Automation, Security Systems, Ticket Machines

 


 

 

For more information, contact your local sales representative.