A quantum leap forward in Data Centers

The typical build cycle for a traditional data center is 2-3 years. This means that what you build today can be obsolete even before becoming operational. The key when creating a strategy for the evolution to be correct and efficient is the agility with which you respond to changes in business strategy, IT requirements, energy needs and costs, and advancing technologies.

A quantum leap forward in energy efficiency, design flexibility and deployment agility of Data Centers

The typical build cycle for a traditional Data Center is 2-3 years. This means that what you build today can be obsolete even before becoming operational. The key when creating a strategy for the evolution to be correct and efficient is the agility with which you respond to changes in business strategy, IT requirements, energy needs and costs, and advancing technologies.

CommScope's Data Center on DemandTM is the answer. It isn't an ISO containerized Data Center. It isn't a simple modular Data Center. It is a purpose-built Data Center that offers maximum energy efficiency, immediate scalability, easy deployment, simplicity, and extremely low maintenance costs.

This solution enables you to build only what you need when you need it, indoors or outdoors.

It features a globally proven technology, based on an advanced patented system of evaporative cooling, which, depending on its settings, can adapt in real time according to the client's requirements and environmental requirements. This system delivers an annual PUE (Power Usage Effectiveness) from 1.03 to 1.06, which means that practically all the electricity consumed in the Data Center is used to power the IT equipment, instead of powering the infrastructure needed to cool and store it. Thanks to this technology, the Data Center on Demand solution delivers high energy efficiency in nearly all environments, without the need for supplementary cooling systems. It's also a great way to help reduce operating expenses.

The Data Center on Demand solution is supported globally by CommScope's service team. From the initial site survey and climactic study, through the installation and commissioning phase and onto maintenance.

CommScope is world-renowned for its vast experience in physical layer infrastructure solutions for Data Centers, especially for its SYSTIMAX® and Uniprise® brands. This knowledge and experience is even further augmented by a growing portfolio of business services and solutions for Data Centers and smart buildings, including iTRACS Data Center Infrastructure Management (DCIM) solutions and Redwood, the space, lighting and analytics solution. 

For more information about this solution, visit  Data Center on Demand™