Axis Introduces Network Loudspeaker for Remote Speaking in Video Surveillance Applications


AXIS C3003-E Network Horn Speaker is a simple-to-install outdoor loudspeaker that provides clear, long-range
speech for remote speaking over a network. When used together with video surveillance, AXIS C3003-E enables
an operator to remotely address people and deter unwanted activity. The loudspeaker is ideal for enhancing video
surveillance installations in outdoor areas such as parking lots, construction and critical infrastructure sites, and public squares. 

AXIS C3003-E Network Horn Speaker

Axis Communications, the global leader in network video, today launched AXIS C3003-E,
the first open standard, network loudspeaker for remote speaking. AXIS C3003-E is simple 
to install and integrate into a video surveillance system or an IP telephony system, making announcements possible from anywhere with network connectivity.

“AXIS C3003-E is really an IoT (Internet of Things) device that provides many advantages because it is connected to an IP network,” says Peter Lindström, Director of New Business
at Axis. “For instance, you can assign a regular phone number to the loudspeaker and simply dial in to it to get heard. It enables integration with just about anything.”


To read the full article, click here.