Emerson

Best availability and highest efficiency among leading rack PDU vendors

Emerson Network Power, a business of Emerson (NYSE: EMR) and a global leader in maximizing availability, capacity and efficiency of critical infrastructure, introduced a new family of  rack power distribution units, including the MPH2 managed rack PDU and the RPC2 communications module. Available now in the United States and Canada, this new generation of the product offers the highest availability and efficiency of managed rack PDUs  among leading vendors, according to independent testing.

 

The MPH2 rack PDU offers one of the highest temperature tolerances in the industry, and together with the RPC2 communications module, offers comprehensive remote management capabilities and real-time monitoring and control of connected loads. This enables the highest availability while allowing IT managers to monitor, predict and manage changes in the data center. Integration with industry standard management and authentication protocols allows the MPH2 to easily integrate with existing IT and communications networks.

 

Read the full article here.