New networked storage, fault tolerant servers allows users to easily add extended and/or archived storage to exacqVision servers

(INDIANAPOLIS) — Exacq Technologies, part of the Security Products business unit of Tyco(NYSE: TYC), a leading manufacturer of video management system (VMS) software and servers used for video surveillance, has released the new S-Series Enterprise line of networked video storage servers.

The new S-Series Enterprise line of networked video storage servers from Exacq Technologies allows users to add extended storage and archived storage to any exacqVision server running the exacqVision Professional or Enterprise Video Management System (VMS) software. In addition, S-Series Enterprise servers can be used to archive video from exacqVision Edge IP cameras. exacqVision Edge is a full-featured VMS that runs directly on compatible IP cameras.

 

By using the S-Series to archive video and audio, users can optimize their network load with scheduled archiving. The S-Series Enterprise includes flexible, user-defined archiving rules to store critical video and audio longer. Additionally, the S-Series allows users to consolidate video archives from multiple exacqVision recorders to one or more S-Series devices.

 

Users can also extend their exacqVision storage without the need for an additional recorder. The S-Series Enterprise is expandable to 80 terabytes on enterprise-class hard drives utilizing RAID 5 or 6 for maximum hard drive reliability. The S-Series Enterprise servers also include redundant power supplies to significantly reduce the risk of a system power failure.

 

With the S-Series networked storage server, exacqVision users will have one unified VMS solution to administer and monitor the storage and recorders. This single user interface reduces the complexity and cost of integrating disparate solutions.

 

For more information on the new exacqVision S-Series Enterprise and other new updates and offerings, go to www.exacq.com.

 

About Exacq

 

Exacq Technologies is part of the Security Products business unit of Tyco (NYSE:TYC), the world’s largest pure-play fire protection and security company. Exacq Technologies designs and manufactures the cross-platform, open-architecture exacqVision video management system (VMS) used in the physical security industry for IP video surveillance. exacqVision is available on factory-installed hybrid and IP camera servers or on commercial off-the-shelf servers. It can also be installed directly on compatible IP cameras, eliminating the need for a separate server. Video from exacqVision servers can be accessed with the free, cross-platform (Windows/Linux/Mac) client, most web browsers and via the free exacq Mobile app available for iPhone, iPad and Android devices. Exacq’s products are available throughout the world.

 

Tyco Security Products and its leading brands conducts business in over 177 countries around the world, in multiple languages and employs over 2,800 employees globally, including research and development, marketing, manufacturing, sales, service and logistics teams in the Americas, Europe, the Middle East, Africa, and Asia Pacific. Our products, built by developers from all product disciplines, consistently allow customers to see more, do more, and save more across multiple industries and segments including healthcare, government, transportation, finance, retail, commercial and residential. Worldwide, Tyco Security Products helps protect 42% of Fortune 500 companies, transportation systems on five continents, 37% of the world’s top 100 retailers, over two millioncommercial enterprises, thousands of students in more than 900 educational facilities, and over five million private residences.