Also announces new iPhone App to see network problems

Fluke Networks OptiView XG V10

EVERETT, Wash. – April 17, 2013 – Fluke Networks today announced a new version of the OptiView® XG v10 Network Analysis Tablet that allows users to simultaneously stress test and diagnose network problems in real-time, as well as a new iPhone App, called HeadsUp™ XG, that receives instant notifications of issues identified by the tablet.


Simultaneous testing is key to quickly isolating intermittent network performance issues, a top concern of more than 75 percent of IT professionals.* With the OptiView XG v10 stress-test capability, network engineers can inject test traffic to measure network performance, examine the traffic’s impact on infrastructure, spot ongoing problems and/or expose many intermittent issues, and map out exactly where problems are located. The new functionality is compliant with International Telecommunications Union standards,** and works in conjunction with a peer or reflective endpoint, such as another OptiView XG or LinkRunner, allowing users to measure end-to-end network performance in terms of bandwidth, latency, jitter, loss and availability up to 10Gbps.


Read the full press release at www.flukenetworks.com.


*Fluke Networks Market Research, 2012

**International Telecommunications Union (ITU) standard, ITU-T Y.1564


Related