Introducing the industry’s first ultra high-resolution 8k camera

Security personnel responsible for the safety of visitors at airports, sports stadiums and other wide-open environments where there is a high risk of terrorist activity, can now rely on a new high-performance Wisenet video surveillance camera manufactured by Hanwha Techwin, to help them detect and forensically analyse any suspicious activity.


“The super high resolution capabilities of the Wisenet TNB-9000 means that large areas can be covered with sufficient pixel density to enable operators to digitally zoom in to see a sharp image of just a small part of the scene,” said Uri Guterman, Head of Product & Marketing for Hanwha Techwin Europe. “This ability to closely zoom in without losing any detail, makes the Wisenet TNB-9000 ideal for applications where installing multiple cameras may be impractical or cost prohibitive.”

Deep learning-based video analytics

The H.265 Wisenet TNB-9000, which utilises a full-size 43.3mm CMOS sensor to capture true 8K images at 15 frames per second, is equipped with deep learning-based video analytics. This simultaneously detects and classifies various object types, including people, vehicles, faces and license plates.

The deep learning-based video analytics is also able to ignore video noise, waving trees, moving clouds and animals, all of which might normally be the cause of false alarms.

In addition to its deep learning capabilities, the Wisenet TNB-9000 has a wide range of built-in Intelligent Video Analytics (IVA), including Tampering, Loitering, Directional Detection, Defocus Detection, Virtual Line, Enter/Exit, Appear/Disappear, Audio Detection and Motion Detection. It also has an audio analytics feature which recognises critical sounds such as raised voices, screams, broken glass, gunshots and explosions, and generates an alert to enable security personnel to quickly react to any incidents.

Additional features

Wisenet TNB-9000 image
  • Digital Wide Dynamic Range (DWDR), helps to accurately produce images in scenes that simultaneously contain very bright and very dark areas.
  • A micro SD/SDHC/SDXC memory slot which allows up to 256GB video or data to be stored at the edge should there be disruption to the network. Video evidence, which might have been potentially lost, can be retrieved when the network connection has been restored.
  • A choice of H.265, H.264 or MJPEG compression, with the cameras’ bandwidth friendly credentials enhanced by WiseStream II, a complementary compression technology which dynamically controls encoding, balancing quality and compression, according to movement in the image.
  • Bandwidth efficiency is improved by up to 99% compared to current H.264 technology when WiseStream II is combined with H.265 compression. As such, WiseStream II reduces the total cost of ownership of a video surveillance system by minimising the storage and bandwidth requirements of high definition cameras.