Alpha Wire Expands Coaxial Cable Offering Sizes Down to 50 AWG

New Micro Coax cable offered in smaller sizes to meet the growing need for signal transmission in confined spaces.

Alpha Wire logo

Elizabeth, NJ, April 6, 2016Alpha Wire recently expanded its Coaxial Cable product line under the Alpha Essentials product family to include Micro Coax sizes from 32 AWG to 50 AWG.  With the addition of Micro Coax, Alpha Wire now offers Coaxial cable products ranging from 10 AWG to 50 AWG.

The new Micro Coax cable line will be offered as standard constructions and are ideal for customers looking for signal transmission options, especially when designs offer limited space for cable routing.  “Alpha’s new 50 Ω Micro Coax line will provide customers with the ability to ensure signal integrity within the increasingly small confines that many designers are working with,” says Hillary Riden, Product Specialist at Alpha Wire. “With an operating temperature range of -70°C up to 200°C, the new micro coax line is ideal for everything from medical endoscopes to industrial inspection applications.”

 Alpha’s Micro Coax cables (32 AWG to 50 AWG) will be in-stock in 100 meter put-ups and available for immediate shipping. Read the full press release.

 

Alpha Wire Micro Coax image
Alpha Wire Micro Coax Cable image