Arecont Vision Introduces Two New MegaDome Camera Series

G3 and G3 RS with the Most Advanced Features in the Surveillance Industry

Dallas, TX (September 25, 2017) – Arecont Vision announces important additions to the MegaDome indoor/outdoor dome camera series that bring new capabilities and easy installation. Both of the new MegaDome G3 and G3 RS (remote setup) dome camera series are Made in USA.
Arecont Vision pioneered the megapixel (MP) dome market in 2009, when MegaDome was the first to offer H.264 compression in an all-in-one camera, lens, and housing solution. Subsequent generations of the series have added many important capabilities and refinements, culminating in the state-of-the-art MegaDome G3 and G3 RS families.

image