AXIS Q1635 Network Camera offers exceptional image quality, with less noise
and motion blur due to the large sensor. The camera is ideal for meeting city surveillance challenges, day and night.

Axis

Axis Communications, the market leader in network video, introduces a new fixed network camera with a 1/2 inch sensor, designed for city surveillance applications. Thanks to its large sensor and the supplied lens, AXIS Q1635 is Axis most light sensitive 1080p HDTV network camera to date. Featuring improved near infrared (IR) sensitivity,
in a range where the human eye cannot see, the camera delivers extremely high-quality black and white images in situations with very little or diminishing visible light – delivering video with less motion blur and low bandwidth consumption.

The camera’s advanced features for optimizing image quality also include Wide Dynamic Range - Forensic Capture, Axis Lightfinder technology, Electronic Image Stabilization, shock detection and defogging, as well as 50/60 frames per second in HDTV 1080p resolution.
“City surveillance requires high quality images that enable the identification of people and objects,” explains Erik Frännlid, Axis’ Director of Product Management. “AXIS Q1635 is ideal for monitoring public places such as squares, parks, streets and alleys, maintaining extremely high image quality in very complex light scenarios during day time and low-light during night time.”

Read the full press release at www.axis.com.

Related