The new compact, rugged and discreet AXIS P39-R Network Camera Series is specially designed for video surveillance in buses, trains, subway cars and other rugged environment vehicles making it ideally suited for citywide transport security. 

Axis Camera

Axis Communications, the world leader in network video, announces AXIS P39-R Network Camera Series offering protection against dust and water and able to withstand tough conditions such as vibrations, shocks, bumps and temperature fluctuations. AXIS R39-R Series also features active tampering alarm function that allows for the detection of tampering attempts such as blocking or spray-painting. 


“The AXIS P39-R Network Camera Series offers high image quality, HDTV resolution, substantial processing performance and edge storage to demanding customers,” says Erik Frännlid, Director of Product Management, Axis Communications. “An important factor in the development of the new AXIS P39-R Series, was to make it easy for customers to upgrade their existing installations. Hence the AXIS P39-R Series shares the same physical interface as the very successful AXIS M31-R Series.” 


Read the full press release at www.axis.com.

Ordering Information

Pricing and stock of the new AXIS P39-R Series will be available from Anixter in late June, 2014.