Axis logo

Axis Communications, the market leader in network video, announces its first corner-mount fixed network camera. The new AXIS Q8414-LVS features a stainless steel anti-grip casing and is extremely impact resistant, supporting the IK10+ 50joules rating as well as the IP66/NEMA 4X rating for water resistance. The 24/7 indoor surveillance camera provides superb image quality both during day and night with capabilities like Lightfinder technology, which enables life-like colors in low-light conditions, and built-in invisible IR LED illuminator for video surveillance in complete darkness. 

“In correctional facilities as well as in psychiatric wards, there is an increasing need to prevent self-harm and avoid internal conflicts among the residents,” says Erik Frännlid, Axis’ Director of Product Management. “We have developed AXIS Q8414-LVS keeping in mind that a surveillance camera should lack ligature points and present an anti-grip design. On top of these features, it should also offer superb video quality during day and night and be extremely vandal resistant.”

The new AXIS Q8414-LVS is ideal for video surveillance of small rooms in premises like correctional facilities, interview rooms, psychiatric wards, and medical observation rooms as well as elevators and stairwells. Thanks to a built-in microphone and the possibility to integrate the network camera into an alarm system via its I/O port, AXIS Q8414-LVS becomes part of the overall surveillance solution, an important tool to protect and secure the safety of the people in high security environments. In addition, privacy masks assure that restricted areas are not monitored for privacy reasons or to protect
the personnel. 

Read the full press release.

axis snp_q8414_lvs_corner