Axis logo

AXIS F Network Camera Series presents a highly flexible, modular network camera series that involves extremely discreet HDTV 1080p cameras with wide dynamic range.

Axis F Series

Axis Communications, the world leader in network video, today introduces a modular camera series that not only gives customers discreet surveillance solutions that provide high image detail, but also great flexibility in choosing the units that are ideal for the installation. The new series is ideal for ATMs (automated teller machines), banks, stores, hotels, as well as rugged environments such as ambulances and police cars.

“AXIS F Series enables great flexibility and discreetness with superb video performance, even in high-contrast lighting conditions,” says Erik Frännlid, Axis’ Director of Product Management. “The series is based on a divided network camera concept, where the camera is split into a lens and image sensor unit, and a main unit. This concept was first introduced in the AXIS P12 Series. When we developed the AXIS F Series, we took into account the feedback we received from AXIS P12 to provide customers with even better solutions.”


The divided network camera concept allows a small sensor unit to be installed discreetly in tight places and the bigger main unit to be placed elsewhere and away from public view. AXIS F Series consists of units that are all sold separately. The series includes AXIS F41 Main Unit and four compatible AXIS F sensor units with different form factors and lens types for different field of views. AXIS F41 Main Unit houses the processor, network, power, SD card slot and other connections, and can connect to one AXIS F sensor unit. Each sensor unit, which consists of a lens and image sensor, comes with the choice of a 3-m or 12-m (10-ft. or 39-ft.) pre-mounted cable for connecting to the main unit.


Read the full article here.