Chatsworth Products Wins Platinum Award for Breakthrough Design in Motive™ Vertical Cable Manager

Tool-less Accessories, Space-Utilization Approach to Cable Management Earned Motive the Highest Honor

image

Chatsworth Products (CPI) was presented the platinum-level award—the highest honor—for its Motive™ Vertical Cable Manager at the Cabling Installation & Maintenance (CI&M) Innovators Award Ceremony on Sept. 25 during the 2017 BICSI Fall Conference & Exhibition in Las Vegas. With a breakthrough design and set of tool-less accessories, Motive is the first cable manager of its kind in the marketplace today.
“Motive further demonstrates CPI’s continued ingenuity in how cables are managed. A lot of time and care were put into the development of Motive to make it the best cable management solution in the industry. It is an honor to be recognized by CI&M for our efforts,” states Duke Robertson, CPI Product Manager of Open Systems.

Drawing from CPI’s extensive experience in cable management and close relationship with contractors and end users, many design elements, both big and small, are integrated into Motive to enhance the user experience.
Motive features a central track system, which allows for infinite, tool-less adjustability anywhere within the cable management space. Additionally, the unique design of the accessories enable a wide range of cable management configurations that allow for direct support of cables with optimal airflow through the cable manager, preparing networks for higher wattage Power over Ethernet (PoE) applications.

More advantages include:

  • Maximum utilization of space
    Central track system provides unlimited adjustability with versatile direct support for cable bundles, while allowing maximum use of interior space.
  • Intuitive, tool-less design
    Accessories attach to the cable manager, enabling support and management of cables, as well as quick attachment, removal and adjustment.
  • Effortless Deployment
    Superior form and functions provide quick and easy moves, adds and changes through intuitive design and tool-less adjustability.
  • Support of current and future cabling needs 
    Versatile configurability and fiber-friendly design mitigate poor cabling practices regarding cable slack, bend radii and cable organization.
image

Also, the front door of Motive features a patent-pending hinge and latch design. With its ability to open from the left or right, the door offers easy push-to-close convenience that securely locks the door into place. Furthermore, an integrated hook on the front door provides a dedicated space for technicians to hang a test meter.
Motive can be used with open two- and four-post CPI Racks and is available in a vast variety of heights, width and configurations, matching all facility requirements. It ships partially-assembled, requiring minimal packaging, storage space and assembly, saving users valuable time and money.