CommScope Extends Next Generation Fiber Frame Portfolio 

CommScope has significantly enhanced its Next Generation Frame (NGF) portfolio by introducing an Enhanced High Density NGF to help data center owners and operators plan and deploy solutions for more bandwidth. The new frame accommodates increased fiber density blocks to seamlessly add fiber terminations without requiring significant changes
to the data center layout while conserving floor space.

Next Generation Frame (NGF) Optical Distribution Frame Solution image

The new frame is seven feet tall and 24 inches deep and can be installed directly next to existing traditional 30-inch wide NGF frames. The pre-terminated fiber blocks eliminate the need to individually plug in hundreds of connectors at the rear of the panel, thus replacing a large number of installation steps. Installers plug pre-terminated MPO assemblies directly into modules at the rear, which distribute trunk fibers into 10G or 40G channels at the front. All pre-populated blocks are factory tested, assembled, and packaged to provide maximum craft friendliness. Pre-terminated blocks with cable stubs are also available.


To learn out more about the Next Generation Fiber Frame, see a dedicated page and download the product catalog.

Related