ComNet Enhances Cybersecurity at the Edge

Introduces Port Guardian Physical Port Lockout

Leeds, UK,  May 23, 2016ComNet Europe Ltd of Leeds in the United Kingdom, part of ComNet Communication Networks, a USA-based manufacturer of transmission and communication networking equipment, has introduced a new Cybersecurity feature in its latest generation of self-managed switches.
The ComNet Port Guardian feature has the capability to physically disconnect a port if unauthorized access is detected.
The value in Port Guardian comes in situations where network access is attempted by disconnecting an IP addressable device on the edge to connect to the network. When Port Guardian senses the disconnect, an SNMP notification is sent to the head end and the effected port is physically locked out, preventing access. The network administrator can reopen the port when the threat is eliminated. This feature also thwarts access through “Spoofing” by disconnecting the port as soon as an interruption is sensed.

logo

This new feature is being added to the newest generation of ComNet SMS products including the CNGE2+2SMS (Anixter Code 660080, 660081 and 660082) and CNGE4+2SMS (release July 2017). The feature will also be available on the new ComNet USA-made Managed Switch line.

According to Steve Clarke, ComNet Europe Managing Director, “Unauthorized access issues or Cybersecurity is a critical challenge facing every network manager today. Your security network with its accessible outside connection, is an easy way to bring down your network. Cybersecurity is not something confined to just a security IP network. Any network can be infiltrated. By introducing this valuable feature on these cutting-edge products, we can provide another unmatched advantage to our partners.”

“ComNet’s goal from day one has been to be a smart and secure choice for transmission products. Our position is that if you are concerned about the long-term success of your application, choosing ComNet ensures it will be,” said Skip Haight, ComNet VP of Marketing. “Port Guardian is another reason ComNet continues to move ahead of our competitors,” Haight continued.

ComNet offers an extensive line of fiber optic, copper and wireless video and data transmission equipment that is uniquely designed to meet the needs of the Security, Intelligent Transportation System, Utility and Industrial markets. 

Related