Corning Plug and Play High Fibre Count Cabling Solution Named Data Centre Cabling Product
of the Year

Corning Optical Communications triumphed at the DCS Awards 2015 winning the Data Centre Cabling Product of the Year. The gala event was held in London in front of a packed audience of data centre professionals and fellow industry peers.

The category shortlist included leading technology companies in the global cabling market, with the winner selected by a wide ranging reader vote among DCS print and online publications from around Europe.


This is the third year running that Corning has taken home a DCS Award and underlines the clear added-value of Corning’s structured cabling solution in the evolving data centre market.

Corning’s Plug & Play™ high-fibre-count MTP connector-based trunk cables address many of the challenges data centres face, such as limited space, heat from densely packed components, and expenses caused by migration to faster networks. Corning’s Plug & Play cables are available with 288, 432, 576, and 864 fibre counts for a significant reduction in physical cable bulk that increases space savings and optimises airflow for cooling energy savings. Plus, the Plug & Play solution is pre-terminated, reducing installation time and cost – and streamlining network moves, adds, and changes for easy scalability.


To find out more, download our high-fibre-count trunk cable features sheet.

The new indoor/outdoor high-fibre-count trunk.