Cut Your Certification Costs by 65%!

banner

Versiv’s ProjX Management System makes setup easy and foolproof … store up to 100 projects and up to 12.000 measurement results in the tester!
Watch the video

Copper and fiber tests now being executed in only a few seconds.
Watch the video

It is important both in the area of both copper and fiber testing. If tested wrong a technician may need to return to site to redo the work.
Watch the video

Stop wasting time and gas driving testers back to the office. Upload and consolidate Versiv test results from remote sites and manage projects from any device with a browser. 
Watch the video

Unique Fault Info function, consolidating decennia of Fluke Networks cabling infrastructure troubleshooting knowledge, provides unmatched diagnostic capabilities. Eliminates time consuming “trial error” testing. 
Watch the video

Visual aids and Graphical User Interface guide users and prevent mistakes from occurring. DTX users have reported spending an average of 20 hours on problems per 1000 links. 
Watch the video

Measuring TCL was previously only possible with laboratory equipment. Evidence is accumulating proving that failed TCL may cause 1GBASE-T and 10GBASE-T to malfunction, even when all other transmission parameters provide good margins above the standard limits.
Watch the video

PoE operation at maximum load is at risk if Resistance Unbalance is not compliant. 
Watch the video

Leading companies worldwide have affiliated with Fluke Networks to leverage the ability of LinkWare Live to streamline the cabling installation and certification process. Typically 3.2 hours per 1000 links are wasted manually editing Cable ID’s in reports that don’t match the specs. 
Watch the video

Final reason why upgrading to Versiv will cut your certification costs – It is time to change …!?!?
Discover more reasons to change downloading the Infographic