Exacq Technologies logo

INDIANAPOLIS - September 16, 2014. Exacq Technologies, part of the Security Products business unit of Tyco (NYSE: TYC), introduces the new EasyConnect automatic IP camera connector feature with the version 6.4 of exacqVision, a video management system (VMS) software used for video surveillance. EasyConnect provides the power of IP cameras with the simplicity of analog. Version 6.4 also includes the new VideoPush video wall feature, updates to the Exacq Mobile app and web browser client, and improvements to Enterprise System Manager (ESM), a health monitoring program for use with exacqVision Enterprise networked video recorders (NVRs).

The new EasyConnect feature allows users to find, address and connect multiple IP cameras to their network automatically. The exacqVision client scans the network to find new IP cameras and the selected cameras are assigned IP addresses and connected to a server. This feature saves time and greatly simplifies the process of adding IP cameras to a modern day, network-based video surveillance solution. EasyConnect supports IP cameras from multiple manufacturers with plans to expand compatibility to most or all of the leading IP camera brands. The initial launch includes support for cameras from Illustra, Axis Communications and Arecont Vision totaling more than 400 cameras.

“As more users are adopting IP video, the addition of EasyConnect is one of the most significant features that has been added to exacqVision,” notes Scott Dennison, Director of Marketing, Exacq Technologies. “EasyConnect simplifies IP video to the point where it’s almost as easy as installing analog cameras.”