How to Choose the Right Door Closer

It’s important to select the right door closer, but there are so many choices out there.

How do you know if you’re advising customers on the right one for their particular application?

Briton Door Closer

Door closers are available with either fixed or adjustable strengths to cater for the size and weight variation of different doors. The wider and heavier the door the greater the force required to close it.

Door closers with adjustable strength are convenient where the size required is uncertain as they facilitate a greater range of adjustment at the time of fitting and remember, fire doors must have a minimum Power Size EN 3 to conform to EN1154 standard.

We help you to make your selection easy

Which Briton door closer is right for your application? Download Briton’s handy guide to door closers to make sure you get it right!

Related