Product Flash JDSU

The only all-in-one handheld solutions for inspecting, precisely testing, and certifying fiber.


December 17, 2014 — JDSU, the industry’s fiber-optic test leader, introduces the newest members of the SmartClass Fiber family. Field service teams are deploying these test tools globally to enhance workflow, quality, and network performance.
As an added benefit, any technician can quickly become
an instant fiber expert.

Integrating automated fiber inspection and optical testing within
a single handheld device, four new models now complement
the existing power meter portfolio:

  • OLT-85 Optical Loss Test Set: Combines both power meter and light source (with four wavelengths) in one handheld instrument to create the essential tool for testing power and link loss and identifying fiber

  • OLP-85 High-Performance Optical Power Meter: Offers the highest accuracy (3%) and best-in-class dynamic range (100 dB) for advanced testing applications

  • OLS-85 Optical Light Source: Up to four wavelengths for quad-singlemode and multimode testing

  • ORL-85 Optical Return Loss Meter: Combines a power meter, light source, and return loss meter in one device to quickly and precisely test CATV, high-speed, and FTTx networks