Milestone Announces Husky M20 – First Model in Next Generation of Adaptable NVRs

Milestone Systems is announcing the Milestone Husky M20 NVR with NVR-optimized Milestone XProtect Professional. This NVR is designed after feedback from the Milestone Community where the need for fast deployable video solutions is rising.

Main Features

Milestone Husky M20  image uk
  • Available in 8- or 16-port variations.
  • The 16-port supports up to 24 cameras.
  • Optional integrated PoE managed switch.
  • Comes with a pre-loaded, NVR-optimized version of XProtect® Professional 2016.

The easiest installation ever

When catering to the mid-market segment, we realize that it’s important for you to offer a proven solution you can trust. Your customers are counting on you, and you want to repay that confidence with a smooth, uneventful installation process. You need a solution where everything works the first time, where you can leave your customer, secure in the knowledge that you won’t be bombarded by calls or complaints because the system isn’t working as it should.

The Milestone Husky M20 is the product you’ve been waiting for. It offers the easiest, most predictable installation process in the industry. The M20 is the shortest route to giving your customers an all-in-one surveillance solution.

The Husky M20 offers

  • Reduced deployment time with integrated Power over Ethernet (PoE) managed switch.
  • A smooth installation process with Smart Start – a series of plug-and-play features that help you connect cameras and configure storage with ease.
  • A predictable installation with no guesswork. We handle the majority of the set-up process, so you get the same good results, every time.

Customers benefits

The new Husky M20 also offers customers a high-performing NVR at an attractive price point.        

  • Replaceable hard disk drives, which help minimize downtime when replacing storage.
  • 200 Mbit/s recording rate, which can handle the latest megapixel cameras.
  • 6th generation (Skylake) Intel® motherboard and processors, which provide high performance local viewing and playback.

Your customers will be lining up for this one. Husky M20 starts shipping November 30 so place your orders today!