Milestone Systems Expands Device Support with More than 1.000 Tested ONVIF Devices


Milestone Systems

Device Pack 7.9 for Milestone XProtect video management software gives Milestone partners and customers extended ability to choose optimal cameras.

COPENHAGEN – May 7, 2015 Milestone Systems, the open platform company in IP video management software (VMS), has released Device Pack 7.9 for partners and customers using Milestone XProtect® security solutions. Device Pack 7.9 has support for 1,012 tested ONVIF devices, all using the same optimized driver. 
  
Support has also been added for Axis Communications’ Zipstream compression technology. This speedy adoption is possible due to the dedicated efforts from Milestone to drive the uptake of open platform technology in the physical security industry.

ONVIF testing ensures quality

The XProtect Device Packs include tested and certified drivers that are optimized to enable the relevant capabilities
of a camera or other hardware device to be managed by the XProtect software. Testing the drivers ensures the highest quality for a video surveillance solution, which is important for total system operability, efficiency and stability. 

Milestone works closely with the device manufacturers in the Camera Partner Program (CaPP) to achieve the optimal interaction between their devices and the XProtect VMS. 
Milestone has always promoted driver standards like ONVIF and remains dedicated to supporting the broadest range
of cameras and devices on the market. 

Advanced compression support 

Device Pack 7.9 also includes support for the Axis Zipstream technology, an advanced mode enabling variable compression as well as variable bit rate. According to Axis, this can reduce the bandwidth up to 50% without major loss in picture quality. 

This technology increases compression when less movement is detected in the video. Beyond reducing the bandwidth, the use of advanced compression technologies like Zipstream can also save disk space on the recording servers in a system. The Milestone VMS has been supporting advanced compression technologies since 2012.

Other release highlights

Extended support for Vivotek cameras has been added. 64 new devices from Dahua have also been added, all based on ONVIF, where the compliance test was done by Dahua themselves. Other vendors with new device support in this release include Pelco by Schneider Electronics, Vicon’s IQEye and Canon.