Device Pack 7.2 for Milestone XProtect video management software gives deep driver support

Milestone Systems

COPENHAGEN – Feb 27, 2014. Milestone Systems, the open platform company in IP video management software (VMS), has released Device Pack 7.2 for partners and customers using Milestone XProtect® security solutions. Device Pack 7.2 has deep driver support for more than 3,000 devices, which means that Milestone has added more than 2,000 supported devices since 2011. This speedy development has only been possible due to Milestone’s dedicated efforts to drive the uptake of open platform technology in the physical security industry.


The Milestone Device Packs include optimized drivers that enable all the relevant capabilities of a camera or other hardware device to be managed fully by the XProtect software. Milestone works closely with the device manufacturers in the Manufacturer Alliance Program (MAP) to achieve the optimal interaction between their devices and the XProtect VMS. This ensures the highest quality for a video surveillance solution - very important for total system operability, efficiency and stability. 


Read the full press release at