Alloc8–X Application & Bandwidth Management Appliance

banner

The Nomadix Alloc8 allows you to monitor, analise and manage all network traffic. Based on the application type, you will understand what type of traffic is crossing your customer network and easyly identify which are the applications types that are consuming the bandwidth. You can easy manage them by defining bandwidth policies in order to provide prioritization and define guaranteed bandwidth limitations to the actual applications that are critical to your organization. The Alloc8 is design for any network environment such from SMB, MDU, hotels, healthcare, retail to larger density such as ISP, datacenters, stadiums, any location were bandwidth is critical.

Why Alloc8–X Application & Bandwidth Management Appliance is the right choice?

Easily Identify and Control Bandwidth

Nomadix control bandwidth icon

Nomadix's Bandwidth Management and Access Gateway appliances allow end users to access the internet without making changes to their networks. "Set and Forget" functionality requires configuration only once during setup without administration oversight from then on.

Monitor Network Activity

Nomadix Monitor Network Activity icon

The Nomadix Alloc8–X Series provides deep insight into users, devices, applications and activities. Its library of purpose-built reports, powerful analytics and predictive recommendations, which automatically make suggestions to resolve network impairments and improve network performance, enable network teams to diagnose and resolve problems up to three-times faster. Purpose-built reports include WAN planning, application performance, network governance and critical IT projects. The health of the network can also be monitored in real time, providing insight into how strategic applications are performing and the amount of bandwidth being consumed across the network.

Analyze and Inspect Traffic

Nomadix Reliable Application Performance icon

This new technology, Nomadix's Alloc8–X Series, allows IT staff to analyze and inspect application traffic at Layer 7 to troubleshoot issues when they arise. Interactive data modeling capabilities provide a better understanding of the health of the network. Intuitive dashboards help operators visualize network activities for all users, applications, devices and locations

Ensure Reliable Application Performance

Nomadix Analyze and Inspect Traffic icon

With the Nomadix Alloc8–X Series in place, applications perform as promised every time. Studies have shown that with the reliable, high-performance Nomadix Alloc8–X Series, user complaints typically drop
by 75% or more. And, with the power to accelerate, shape and cache application traffic in a single solution, network operators can now guarantee that their most important applications will always perform at their best.