Nomadix Inc. Launched the AG 2500 Access Gateway 

logo

For small-to-medium-sized venues.

Nomadix Inc. launched the AG 2500 access gateway – its newest high-performance solution that extends a wired or Wi-Fi network to create a visitor-based network (VBN). Designed for small-to-medium-sized venues, such as hotels with fewer than 150 rooms, the AG 2500 supports up to 500 simultaneous mobile devices at a very competitive price. With the release of the new gateway comes the latest version of the NSE (Nomadix Service Engine); version 8.9 supports not only the AG 2500 but also the Nomadix AG 5800 and AG 5900 access gateways, which service larger properties.

AG 2500 access gateway  image

With the introduction of the AG 2500, Nomadix is providing a new modular configuration that gives customers the flexibility to tailor the gateway to their individual requirements and reduce their overall total cost of ownership.
The AG 2500 is offered with a robust base configuration that includes a 400 device count. Customers can upgrade the AG 2500 to 500 devices, with the ability to add the following software modules:

  • Hospitality PMS Software Module.
  • High Availability Failover Software Module.
  • Load Balancing Software Module.
  • Bandwidth Management Software Module (included in the Anixter Codes 900129 and 900142).

The AG 2500 is built upon an Intel processor that offers high performance, low power consumption, reliability, longevity, and built-in flash memory.
The AG 2500 provides customers with an access gateway that will satisfy many value-based visitor network needs – while offering the flexibility to add features suitable for applications requiring more sophisticated bandwidth management, resiliency and PMS monetization.

“One of the most common issues we continue to hear about from properties large and small is the challenge of keeping up with the growing bandwidth demands being placed on them by mobile devices – all of which want access to the visitor network,” said Nomadix President Fred Reeder. “As a company, we continue to innovate and improve our solutions using advanced technology to solve these challenges. Our newest gateway utilizes the best processor available to ensure that smaller properties who offer internet access can do so in an effective yet economical manner. And our latest software refines the bandwidth management process even further, providing venues and properties with the technology they need to enhance the guest experience.”

Capabilities

  • Effortless creation of a VBN.
  • Effective bandwidth management, control and allocation to maximize use of existing bandwidth.
  • Ability to easily add guests onto the network.
  • Scalability to accommodate small-to-large-sized networks in a range
    of locations, from coffee shops to hotel resorts to convention centers.
  • Flexible deployment that is adaptable to the needs of the guest user.
  • Modular pricing scheme that provides a lower barrier of entry and the flexibility to reduce overall total cost of ownership.

Why The AG 2500 Is The Right Choice?

  • Next generation platform for speed and durability.
  • Fast authentication and secure access control.
  • Flexible billing options and seamless integration.
  • Bandwidth management.