Nomadix Introduces the EG 6000 Gateway

Newly Doubling Performance of Prior Generation Solutions Setting a New Standard in Throughput

Nomadix Inc., the innovator and pioneer of bandwidth management and public access gateways, has announced its newest gateway, the EG 6000, which extends bandwidth for Wi‑Fi and/or wired networks supplying public internet access. Due to a next-generation CPU, the EG 6000 offers 6Gbps of sustained bandwidth, making it the highest‑performing platform in Nomadix’s family of bandwidth management and access gateways.

The EG 6000 (Edge Gateway), announced at HITEC in June 2018, is the latest and most advanced bandwidth management gateway in the Nomadix lineup.

This new gateway is designed to be at the network edge for Multi-Dwelling Units (MDUs) including apartment buildings, condominiums, student housing and assisted living facilities.
The EG 6000 represent a new, additional product line from Nomadix and is not a replacement of the AG series of gateways.

It will be ready to ship after May 1, 2019.

Click below for features and technical specifications for the new EG 6000.

EG 6000 Gateway