OPTEX to Extend Its New Laser Range And Certification Program

 With flexible installation and IP connectivity, the new range continues to define OPTEX as an innovative leader within the security industry. 

Masaya Kida, Senior Manager Product and Business Planning Department, OPTEX

image

Leading sensor manufacturer OPTEX has announced the global roll out of its outdoor and high-resolution indoor laser sensor RLS-2020S, complementing its next-generation REDSCAN mini sensor that features a 20x20m detection range.

The new sensor will be launched in North and South America in December and in Europe, Middle East and Africa (EMEA), Dubai’s INTERSEC (22nd – 24th January 2017) is the chosen exhibition for the product’s launch.

The S-model features an enhanced microprocessor that provides more powerful sensing capabilities. In indoor environments, it can be set up to identify fast travelling objects or very small objects. This information can be relayed to a Video Management Software (VMS) to provide a quicker, more accurate response. The sensor is PoE compliant, and can send alarms via traditional relay outputs or by using its IP based Redwall event code that is integrated with all major VMS platforms.

Read the full article here.

Related