The Mighty Mo 20 Hexguard is Now Available! 

Ortronics® is excited to introduce the Mighty Mo 20® Hexguard™ Cabling Protection! 

The Mighty Mo 20 Hexguard is Now Available!  image

Ortronics introduces the Mighty Mo 20® Hexguard™ Cabling Protection. The new Mighty Mo Hexguard cable management accessory is the latest addition to the innovative and comprehensive Mighty Mo 20 Cable Solutions for networks requiring flexibility, efficiency, and superior design.The Mighty Mo 20 Cable Management System is built to maximize network performance by minimizing signal loss caused by improper cable support. The unique design of the Hexguard shields cables in the channel sidewall, allowing cables to safely pass from the inside to the outside. The easy to install Hexguard allows proper bend radius on both sides of the sheet metal hex. 

Features

  • Snap fit over existing cables
  • Can be used singles sided or dual sided
  • Shortens rack to rack cable lengths
  • Provides proper bend radius for fiber cables

Benefits

  • Snap fit over existing cables
  • Protects cables and allows channel rail pass thru
  • Supports up to 48 Cat6 cables
  • Provides proper bend radius for fiber cables

Resources