Panduit’s New Net-Verse™ Cabinets Offer a Scalable and Cost Efficient Solution for Data Centre and Enterprise Applications

banner

Panduit, a world-class developer and provider of leading-edge physical infrastructure and connectivity solutions, announced the availability of Net-VerseTM Cabinets in Europe. Net-VerseTM Cabinets are a highly flexible cabinet design for applications that require scalability, security and cost efficiency in On Premises & Colocation/Cloud Data Centre or Enterprise deployments. Adaptive design features include fully adjustable equipment rails that cater to both server and switch applications. The cabinets have enhanced physical security features such as multi-point locking front and rear doors and locking side panels. For high density compute environments, its versatility is further supported by two full length combination PDU/lashing brackets that can accommodate up to 2 PDU’s, including Panduit’s recently launched Smartzone G5 Intelligent PDU, on each side of the cabinet.

“Panduit’s Net-Verse Cabinets offer customers a flexible and cost efficient cabinet solution for enhanced data centre agility and scalability, especially in the colocation and cloud environments,” said Sander Kaempfer, Business Development Manager, Data Centre, Panduit EMEA.

The new Net-VerseTM Cabinets compliments Panduit’s line of configurable and energy efficient Net-Access™ Cabinets and are designed for applications that require optimal thermal management within the latest containment environments. Net-Verse Cabinet front and rear doors provide a generous 69% opening for optimized airflow.

For more information