Proxim Announces the QB-10100 Series of High Capacity Point to Point Products

Introducing Tsunami® QB-10100 Series banner

Silicon Valley, CA, February 8, 2016 Proxim Wireless Corporation, a pioneer and global leader in advanced Wi-Fi, point to point (PtP), and point to multipoint (PtMP) wireless systems, is introducing the carrier-class, very high capacity Tsunami Quickbridge® 10100 series
of products.

The QB-10100 series represents Proxim’s highest speed PTP products, supporting up to 633 Mbps of data throughput. The useable throughput is achieved with a mere 866 Mbps of RF data rate, delivering an industry-leading 73% efficiency. With the recent release of the QB-835 at the low end of the PTP portfolio, with throughputs as low as 25 Mbps, Proxim has expanded its PTP offerings dramatically. 

Related